EN - product guides

In this section Product Instructions, you will find step-by-step instructions for item products.
These can be opened as required before or during installation, e.g. on a mobile device at the workbench.
The processing time per module depends on the product and varies.
Do you have any questions, feedback or requests for new interactive instructions? We are looking forward to your e-mail to academy@item24.com!
These can be opened as required before or during installation, e.g. on a mobile device at the workbench.
The processing time per module depends on the product and varies.
Do you have any questions, feedback or requests for new interactive instructions? We are looking forward to your e-mail to academy@item24.com!
Work Bench System
Flexible Conduit Set D40 60x60 is a versatile solution for routing cables in various different ways.
The new item drawer system makes it quick and easy to assemble drawers.
Mit der Interlock-Lösung erhöhen Sie die Arbeitssicherheit von Schubladenschränken und Regalen mit ausziehbaren
Tabletts.
The friction joint 8 E is an economical solution for designing customised pivot arms and swivelling control panels.
Build a table frame step by step using the table column set 8 80x40 K.
Build a table frame step by step using the table column set D40/D30 K.
The lockable Drawer S1 H70 can be installed under a table top or on profiles.
How do I control and program a work table? How do I set it up? This module shows it.
Automation System
This module shows the step-by-step assembly of the linear unit KLE 5 40x40 LR.
The module shows the installation, programming and commissioning of the stepper motor.
Wie verkabel ich einen Schrittmotor mit dem StarterKit? Dieses Modul zeigt es.
Step-by-step instructions: Toothed belt disassembly and assembly, setting the toothed belt pre-tension, carriage
This module shows the maintenance of the Linear Unit KRF 8 80x40 ZR.
Step-by-step instructions: Toothed belt disassembly and assembly, as well as setting the toothed belt pre-tension.
The instructions show the commissioning step by step.
This module shows the step-by-step assembly of the Profile Fastening Set 6/8 80x60
This module will lead you step by step through the installation process of Controller BL1-04/C.
This module shows the step-by-step assembly of the Parallel Drive Set 6 60 D12-1 SE 60.
The connection on the motor side must be individually adapted to the motor to be selected. For this purpose, the corresponding components must be machined.
This module shows the step-by-step assembly of the linear unit LRE 8 D14 80x40 ZU 40 R25.
This module shows the step-by-step assembly of the Linear Unit KLE 6 / KLE 8.
This module shows the step-by-step assembly of the linear unit LRE 8 D14 80x40 ZS.
Conveying Technology
The item Railing System 8 D8 gives you the design freedom you need to safely guide goods of all kinds in any situation.
The item centre drive can be used to position the motor underneath the conveyer.
This module shows the step-by-step assembly of the belt conveyor 8 40 D.
This module will lead you step-by-step through the assembly process of the Timing Belt Conveyor 8 40 D.
This module shows the step-by-step assembly of the double flat belt conveyor 8 40 D.
This module will lead you step-by-step through the assembly process of the double timing belt conveyor 8 40 D.
Lean Production Building Kit System
The Release Unit D30 H8 is the ideal partner for front shooters for all item roller conveyor types.
With the Suspended Conveyor System, components that take up a lot of space in a KLT-carrier can be transported in a suspended position.
This instructional video shows how curves are installed for the item Suspended Conveyor System.
This instructional video shows how the transfer bracket is installed for the item Suspended Conveyor System.
This guide shows how to install a manual trigger mechanism that releases the transport of a carriage via a Bowden cable.
This instructional video shows how the separator is installed for the item Suspended Conveyor System.
This module shows step-by-step instructions for building a chain-synchronised carriage in the Karakuri/LCA field.
You want to get to know the absolute basic elements of the LPS and their application? Then take a look at this module.
Build a practical beverage shelf.
The bearing block serves as a precise and smooth-running pivot bearing for larger and heavier frame parts. Supplemented by up to three rotary dampers, the bearing block provides a controlled and safe rotary movement.
You want to know how to realise a door solution with the Hinge D30-85 FP? Then you have come to the right place!
MB Building Kit System
The hinges Al light are suitable for swing doors and flaps in profile construction or made from panel elements.
Modular system for aluminium hinges with high load capacity, suitable for heavy doors, flaps and pivoting...
The item latch keeps doors securely closed and makes operation easier thanks to the integrated handle.
The Magnetic Catches are preferably suitable for locking swing and sliding doors.
With the Lifting-door system, lifting doors up to a width of 2m and a total weight of 35kg can be realised.
Sliding Door 8 32x18, Catch makes it possible to open and close several door segments made from Clamp Profiles 8 32x18 simultaneously
Impact Buffer D15x15 M4x12 acts as a catch and also helps minimise the risk of fingers becoming jammed in sliding doors
Sliding Door 8 32x18, Fixing Plate is used to hold the door segments of a sliding door made using Clamp Profiles 8 32x18 in one place
Sliding Door Lock 8 features an integrated grip that also releases the door latch. When pulled shut, the slim locking piece engages with the space-saving lock case, which is fastened to the Line 8 profile groove of the door frame. Only a very small door gap is created.
Sliding Door Magnetic Catch 8 is a magnetic holder for sliding doors.
The new item drawer system makes it quick and easy to assemble drawers.
With the safety fastening set Multiblock 8, you can quickly, easily and safely install panels in accordance with the Machinery Directive.
The Multiblock 8 PA 0/5 mm makes it quick and easy to install perforated sheets.
The Clamp-Multiblock 8 PA allows you to quickly and easily install panels without the need for further processing.
Attach Profile 6 to Profile 8 – with the Automatic-Fastening Set 6/8.
Step by step: how to mount a Castor D65 swivel on the end face of a Profile 8.
Step by step: how to mount a Castor D75 swivel on the base plate.
Step by step: how to mount a Castor D75 fixed on the base plate.
Step by step: how to mount a Castor 140x110 swivel and fixed on the frame.
Dieses Video zeigt die Montage der Zustellung 8 40 gegenläufig mit digitaler Positionsanzeige.
How do I mount steel mesh with the steel mesh fixing block? This module shows you how.
How do I mount panels with the panel fixing block? This module shows you how.
How do I build a Fixed Panel with Clamp Profile for Guard 8? This module shows you how.
How do I install a Fixed Panel with Polycarbonate for Guard 8? This module shows you how.
How do I build a Guard Section with Steel Mesh for Guard 8? This module shows you how.
Automatic-Fastening Set 8 S joins two Line 8 profiles at a right angle to create a connection that is particularly resistant to displacement, torsion and bending.
Telescope 8 80x40 is a heavy-duty strut of adjustable length. TheTelescope Inner Profile 8 80x40, which is mounted in a plain bearing, is attached here using the Telescope Securing Set 8 80x40.
Step-by-step assembly of the Swivel Castor D125 120×40 to a Series 8 transport frame.
Mit der Interlock-Lösung erhöhen Sie die Arbeitssicherheit von Schubladenschränken und Regalen mit ausziehbaren
Tabletts.
With the ball joints, you freely align profiles and accessories in two dimensions.
Telescope 8 40x40 is suitable for struts with adjustable length for height or inclination adjustments of operating equipment.
The telescope 8 80x40 is a load-bearing strut with an adjustable length and is locked using the telescope locking plunger 8 80x40.
The T-Slot Slider 8 80x40 uses the t-slot groove 8 to guide a robust slide element with plain bearings.
A spindle adjustment for feeders, measuring assemblies, limit switches and fixtures.
For the construction of sliding doors made of frameless panel elements that are guided in the t-slot groove with sliding pieces.
Smooth-running and stable sliding door elements for safety guards.
The item Access Door system is based on components that have been carefully coordinated to produce highly functional door solutions.
The Universal Holder 8 K is a three-part system for covered cable routing along the groove.
The roller shutter system is designed for the installation of manually operated roller shutters, for example, for closing cabinet systems, control panel...
Panel-Clamping Strips are ideal for retrofitting panel elements (primarily made of Acrylic Glass, PET-G or Polycarbonate) into an assembled profile frame.
Particularly easy-to-use connecting element for two parallel profiles of Line 8.
The edging strip 8 K is used to retrofit panel elements into a closed profile frame.
The infinitely adjustable feet are suitable for structures of all kinds. A ball and socket joint compensates for slopes.
The apparatus castors are available in several sizes as swivel castor, swivel castor with double locking device (brake for wheel...
Perfect for doors: If panel elements are to be fixed in the profile grooves, the corners do not have to be notched with the central-fastening set.
Stable fastening plates for accommodating Adjustable Feet, Castors and other elements.
The angle sets 8 serve as a non-positive connection of profiles without the need for machining.
Universal, friction-locked connection of all profiles of a series with the possibility of subsequent displacement, as the...
Universal, non-positive connection of all profiles of a series with the possibility of subsequent displacement, as the profiles can be...
Mitre-Butt-Fastening Sets are suitable for connecting two profiles at an angle.
The item Standard-Fastening Set connects two profiles at right angles with high strength. Its connecting plate is used for optimum force transmission and ensures correct positioning and torsion-resistant fixing.
To enable panel elements to be fixed in the groove without an additional recess in the area of the connecting elements, the standard connecting set 8 K is particularly compact.
The Automatic-Fastening Set 8 NO is suitable for closed grooves.
With the Diagonal Strut Set 8 300x30 you increase the load capacity of horizontally running profiles in an elegant and simple way.
The hinge connects profiles at any angle up to 180°. Removing the spacer rings creates a rigid angle element.
Clamp-Profile Fastening Set ensures a correctly positioned corner connection for the profiles.
Fastening set 8 40x40x40 can be used to connect two or three profiles at 90°.
Additional support for loaded profiles: With the item Pin Element, you can additionally secure a non-positive connection with a positive fit.
Stand Foot Set 8 St 160x160 combines optimum protection with a compact design and is ideal for use with freestanding enclosures and guards.
item Adhesive Multiblocks are the solution for quick, easy and flush fixing of surfaces in profile frames.
Additional protection for sensitive areas! With the barrier tape you limit the
access and avoid carelessly entering work areas.
Sealing profiles fasten panel elements of different thickness in the profile groove 5, 6, 8 or 12. The permanently elastic strips of TPE seal the groove edges and make cleaning easier because neither moisture nor dust can collect in the groove.
With the modular conduit system, individual conduits for cables and hoses can be constructed.
Fasteners for fixing a profile at an angle of 45° when constructing joints and trusses.
Rebate Profile for universal fastening of various elements to Profiles.
Bed Plate Profiles 8 for producing areas of any size with groove 8 and modular dimension 40 mm.
The Automatic Butt-Fastening Sets can be used to connect the end faces of two profiles from the same Line without mechanical processing.
The Universal-Butt-Fastening Sets can be used to connect the end faces of two profiles from the same Line.
Face Fastening Set 8 is used to create a rigid angled connection between two profiles whose grooved sides face each other.
Smart Products
This module shows the installation of the LED strip RGB 24V with accessories.
Der Multi-Segment RGB LED-Streifen ist ein flexibles, durch IO-Link ansteuerbares, LED-Band.
How do I configure the basic settings for the Multi-Segment RGB LED Strip Controller DIN/AIN 24VDC in the web interface? This module shows you how.
How do I configure the segment mode for the Multi-Segment RGB LED Strip Controller DIN/AIN 24VDC in the web interface? This module shows you how.
How do I configure the level mode for the Multi-Segment RGB LED Strip Controller DIN/AIN 24VDC in the web interface? This module shows you how.
How do I install the electronic Release Unit DIN/DOUT 24V? This module shows you how.